DIGITAL MULTIMETER

Sign Up For Safety

Receive our free e-mail newsletters that are packed with insights and tips from safety experts. Want to make a difference in your company? Sign up today.

Choosing a Digital Multimeter

These modern-day tape measures consolidate the functions of voltmeters, ammeters, and ohmmeters into a single unit.

As one of most widely-used electronic testing instruments, the digital multimeter (DMM) is more commonly known as the modern-day tape measure. But instead of being able to handle a single function (i.e., linear measurement), DMMs consolidate the functions of multiple instruments, such as voltmeters, ammeters, and ohmmeters into one unit.

DMMs are used in electrical engineering design, maintenance, quality control, inspection, and/or any application requiring electrical servicing and diagnostic testing. A basic DMM works with energized and de-energized electrical circuits and measures alternating current (AC), AC voltage, direct current (DC), DC voltage, resistance, continuity, and diodes. Advanced models measure capacitance, frequency, temperature, pressure, and vacuum (special accessories are required for some of these measurements).

SHOP RELATED PRODUCTS

Electrical Power Testing
Electrical Power Testing
Digital Multimeters
Digital Multimeters
Test Lead Connectors
Test Lead Connectors

Choosing a Multimeter

When selecting a DMM for a specific application, consider these three points: 

  • Resolution refers to how fine a measurement a meter can make. By knowing the resolution of a meter, you can determine if it is possible to see a small change in the measured signal. The terms digits and counts are used to describe a meter’s resolution. DMMs are grouped by the number of counts or digits they display. A 3 ½-digit meter can display three full digits ranging from 0-9 and one-half digit, which displays only a “1” or is left blank. A 3 ½ digit meter will display up to 1,999 counts of resolution and a 4 ½ digit meter can display up to 19,999 counts of resolution. Some DMMs may have enhanced resolution offering higher counts within their digit range.
  • Accuracy is the largest allowable error in the readings. It’s an indication of how close the DMM’s displayed measurement is to the actual value of the signal being measured. Accuracy is generally expressed as a percent of the reading. An accuracy of one percent of the reading means that for a display of 100 volts, the actual value of the voltage could be somewhere between 99 and 101 volts.
  • Autoranging (or “dialing”), is a useful feature that allows the user to quickly move from the instruments’ various measuring scales while maintaining accurate readings.

Another important consideration to factor in when selecting a DMM is whether it is a True RMS (root mean square) meter or not. True RMS meters allow non-sinusoidal AC signals to be accurately measured. The typical DMM is not a True RMS meter, and the former will produce misleading voltage readings when used to measure anything other than DC signals or pure sine wave AC signals.

Regardless of which multimeter you chose, electrical test equipment should be used with caution, respect, and maintained in accordance with the manufacturer's guidelines. As with all electrical test equipment, individuals using a DMM should receive training in its proper operation.

It’s important to use extreme caution anytime you work with current (AC or DC) and voltage. To avoid catastrophic consequences, an electrical safe work program should be established and followed whenever working with electricity.

Banner

 

Find even more information you can use to help make informed decisions about the regulatory issues you face in your workplace every day. View all Quick Tips Technical Resources at www.grainger.com/quicktips.

Think Safety. Think Grainger.®
Grainger has the products, services and resources to help keep employees safe and healthy while operating safer facilities. You’ll also find a network of safety resources that help you stay in compliance and protect employees from hazardous situations. Count on Grainger for lockout tagout, fall protection equipment, confined space products, safety signs, personal protective equipment (PPE), emergency response and so much more!

DISCLAIMER:The information contained in this publication is intended for general information purposes only and is based on information available as of the initial date of publication. No representation is made that the information or references are complete or remain current. This publication is not a substitute for review of the current applicable government regulations and standards specific to your location and business activity, and should not be construed as legal advice or opinion. Readers with specific questions should refer to the applicable standards or consult with an attorney.

©2016 W.W. Grainger, Inc.