Padlocks

Sign Up For Safety

Receive our free e-mail newsletters that are packed with insights and tips from safety experts. Want to make a difference in your company? Sign up today.

TYPES OF PADLOCKS

Padlocks are detachable locks that normally incorporate a u-shaped bar that’s hinged at one end and designed to be passed through an opening of a hasp or a link in a chain to protect against unauthorized use, theft, vandalism or harm.

They are comprised of three basic components: the shackle, body and locking mechanism.

Shackle: Most often a loop of metal (u-shaped bar) that opens up to lock and unlock the padlock - available in varying lengths and diameters to fit a variety of needs. There is a rather unique style of lock (see the single-post shackle padlock below) that uses a straight shackle.

Body: The solid part of the padlock that contains the locking mechanism.

Locking mechanism/cylinder: Locks usually have a keyway where the key is inserted, or they may use a type of rotary mechanism or dial.

SHOP RELATED PRODUCTS

Combination Lock
Combination Locks
Keyed Padlock
Keyed Padlock
Padlocked Accessories</p>
<p>
U-Shaped Padlocks

Types of Padlock Styles

Padlocks are used in virtually every business, organization and home. In order to fill the needs of these different groups, a wide variety of options and styles have been developed. Below is an overview of some of the most common types of padlocks:

Breakaway shackle: A lock that features a scored shackle that will break when struck by a hammer or other substantial object. This padlock would be used in applications where the lock may need to be removed rapidly for emergency response like on sprinkler hose shut-off valves and fire hoses.

Combination: A lock that uses a rotary dial or series of buttons to unlock the device rather than a conventional key.

Combination with key control: A lock with key control that can be opened with a key or a combination. This type of lock is typically used in schools and locker rooms. The control key is capable of opening all the combination locks in that set.

Guarded/shrouded/shielded: A lock that has solid metal guards that protect and surround the shackle on both sides, leaving only the top of the shackle exposed. The guards make it much more difficult to cut the shackle with a bolt-cutter.

Government: Locks made to meet exacting U.S. government production standards such as Commercial Item Description (CID)-A-A-59486, CID-A-A-59487 and CID-A-A-1928.

High security: A lock that typically has one or more of the following options to increase its level of protection:

  1. Hardened steel shackle for cut resistance
  2. Shrouded shackle to protect against cutting and prying
  3. Pick-resistant key cylinder
  4. Reinforced locking mechanism to resist prying

Laminated: The body consists of multiple pieces of metal stacked on top of each other to form a tough, tamper-resistant lock.

Lockout: Locks designed specifically for use in lockout programs that often have a provision on the lock to write the users name and come with only one key to limit access to the lock. For more information on lockout padlock requirements, see Padlocks for Your Electrical Safety Program. For additional information on OSHA’s Lockout/Tagout standard, see Lockout Tagout Systems and Standards.

Single-post shackle: Unlike the other styles discussed here, this lock uses a single post rather than a U-shaped shackle. These are used on vending machines, utility valve equipment, meters and wherever a less accessible shackle is desired.

Weather resistant: Locks that have either a shroud to protect the lock from the elements or are constructed from weather-resistant materials such as stainless steel. Although regular locks will work outside for a period of time, they tend to rust or corrode over time to a point where they can no longer be opened with the key or combination sequence.

Keying Options

For most applications, the typical padlock that comes with two keys works well. However, there are many applications where different keying options are required. The most common keying options are:

Keyed alike: All the keys open all the locks in a set of padlocks. Every key and every padlock is exactly the same.

Keyed different: Each padlock has a unique key(s)  two keys that only open that lock and will not open any of the other locks within the set.

Master keyed: Locks are keyed different padlocks with the addition of a single master key that can open all the locks in a set. The keys that come with the locks can only open that one lock, but an additional master key will open all the locks in the set. The master key and the master keyed padlocks must be ordered at the same time.

Rekeyable: The cylinder in rekeyable padlocks can be removed in order to (a) change the pinning or (b) replace the original cylinder with a new one, restoring security quickly and economically. This is ideal for situations where keys are lost or stolen.

Interchangeable core: These provide an instant security solution because they do not require disassembly to remove the core (cylinder). The control key fits into the padlock just like the user key, but actuates the interchangeable core retaining mechanism to allow the removal and replacement of the core (cylinder).

Non-removable key: The key cannot be removed from the padlock when the lock is open. This helps prevent users from accidentally leaving the padlock in the open position.

Reserved key system: The reserved key system is not available to the general public but is a system where key blanks are cut and supplied directly through padlock distributors when requested by registered end-users. These locks are typically used by the government and some larger companies.

Materials of Padlock Construction

Padlocks are made in a variety of metals and even plastic. Some of the common materials and applications for those materials include:

Plastic: Typically used in a light security situations where tampering isn't expected to occur.

Aluminum: Generally used in light security situations. The aluminum bodies are often anodized in different colors, allowing color coding of lock systems.

Brass: More durable than plastic but are not as tamper-resistant as heavier steel padlocks. However, they do hold up to the elements and are often used as an inexpensive, weather-resistant light security lock.

Solid steel/case hardened steel: Very durable, cut-resistant materials. These types of locks are typically used in higher security applications and are often chrome or zinc-plated to help resist corrosion.

Stainless steel: Very durable locks and generally hold up to the elements better than solid steel.

Titanium: Extremely durable metal resists corrosion and is lightweight in comparison to solid and stainless steels. These are typically used in higher security applications.

Commonly Asked Questions

Q. Can I get replacement keys for my padlock?

A. If you have the key number that is stamped on the key itself, a locksmith may be able to get a replacement key for you. If you do not have the key number, it may be possible to have a locksmith make a replacement key. If the lock is from a supplier that Grainger works with, we should be able to assist. Please call 888-361-8649 and request our Custom Product Center at extension 2879999.

Q. Are master keyed and keyed alike locks the same?

A. With master keyed locks, the individual keys will only open one lock but there is a separate master key that can open all the locks in a group. With keyed alike locks, every key in a group will open every lock.

Source

Master Lock® Safety Knowledge Center (Rev. 8/2018)

Find even more information you can use to help make informed decisions about the regulatory issues you face in your workplace every day. View all Quick Tips Technical Resources at www.grainger.com/quicktips.

Think Safety. Think Grainger.®
Grainger has the products, services and resources to help keep employees safe and healthy while operating safer facilities. You’ll also find a network of safety resources that help you stay in compliance and protect employees from hazardous situations. Count on Grainger for lockout tagout, fall protection equipment, confined space products, safety signs, personal protective equipment (PPE), emergency response and so much more!

DISCLAIMER:The information contained in this publication is intended for general information purposes only and is based on information available as of the initial date of publication. No representation is made that the information or references are complete or remain current. This publication is not a substitute for review of the current applicable government regulations and standards specific to your location and business activity, and should not be construed as legal advice or opinion. Readers with specific questions should refer to the applicable standards or consult with an attorney.

©2016 W.W. Grainger, Inc.