Safe Forklift Operation: Train (and Train Again)

Sign Up For Safety

Receive our free e-mail newsletters that are packed with insights and tips from safety experts. Want to make a difference in your company? Sign up today.

Safe Forklift Operation: Train (and Train Again)

A forklift in motion is a safety risk in motion. Ensure your operators have received the proper forklift safety training.

The Occupational Safety and Health Administration (OSHA) defines a powered industrial truck as a mobile, power-propelled truck used to carry, push, pull, lift, stack or tier materials. There are many different types of powered industrial trucks, and each type presents different operating hazards. The most familiar powered industrial trucks are commonly known as pallet trucks, rider trucks, forklifts or lift trucks. Forklifts/lift trucks are extremely useful in the workplace, as long as they are safely used by trained operators.

Background

OSHA revised the Powered Industrial Truck Standard (29 Code of Federal Regulations [CFR] 1910.178) in 1999 to include training requirements for employees who operate powered industrial trucks. Yet powered industrial truck violations annually remain among OSHA’s Top Ten most frequently cited standard violations. One of the major compliance issues is failure to train.

Forklift Safety Training Requirements

Employers must develop and implement a training program based on the general principles of safe truck operation, the types of vehicle(s) being used and the hazards they create, and the general safety requirements of the OSHA standard. Trained operators must know how to do the job properly and safely, as demonstrated by workplace evaluations. Formal (lecture, video, etc.) and practical (demonstration and practical exercises) training must be provided. Employers must also certify that each operator has received the training and evaluate each operator’s performance at least once every three years.

Training Program Content

Operators must be initially trained in the following truck-related and workplace-related topics:

  • Truck Related:
    • Operating instructions, warnings and precautions for type of truck
    • Similarities and differences with automobiles
    • Control and instrumentation location and use
    • Engine or motor operation
    • Steering and maneuvering
    • Visibility
    • Fork and attachment limitations and use
    • Vehicle capacity
    • Vehicle stability
    • Vehicle inspection and maintenance
    • Refueling or charging batteries
    • Operating limitations
    • Other operating instructions, warnings or precautions listed in the operator's manual
       
  • Workplace Related:
    • Surface conditions where truck is used
    • Load composition and stability
    • Load stacking, unstacking and transport
    • Pedestrian traffic
    • Narrow aisle and restricted area operation
    • Operation in hazardous locations
    • Ramp and sloped surface operation
    • Unique or potentially hazardous conditions
    • Operating the vehicle in closed environments
       

Because powered industrial trucks are manufactured by different companies with various models available, the training must be specific to the operating characteristics of the specific powered industrial truck the employee will be using.

If an operator was previously trained on one of these topics, and the training is appropriate to the truck and working conditions encountered, additional training on that topic is not required if the operator has been evaluated and found competent to operate the truck safely.
 

Evaluation and Refresher Training

An evaluation of the performance of each powered industrial truck operator must be conducted every three years. OSHA requires that formal refresher training be conducted under certain circumstances. There is no set frequency, but employers do need to retrain when:

  • The operator has been observed to operate the vehicle in an unsafe manner
  • The operator has been involved in an accident or near-miss incident
  • The operator has received an evaluation revealing that the operator is not operating the truck safely
  • The operator is assigned to drive a different type of truck
  • A condition in the workplace changes in a manner that could affect safe operation of the truck

Certification

The employer must certify that every operator has received appropriate training, has been evaluated and has demonstrated competency in performing the operator’s duties. The name of the trainee, date of training, evaluation date and name of the person(s) performing the training or evaluation must be included on the certification.

Commonly Asked Questions

Q: What is the stability triangle?

A: The majority of counterbalanced industrial trucks have their weight supported on three points. Even on a four-wheeled truck, the front two drive wheels are two points on the stability triangle, while the back two steering wheels, which are connected on a central pivot, support the weight at the rear and make the third point. When these three points are connected with imaginary lines, the stability triangle is formed.

The stability triangle is useful in explaining the stability of a powered industrial truck. An unloaded truck on a level surface will have a center of gravity in the middle of the stability triangle. As a load is added to the truck, or if the truck is on an inclined surface, the center of gravity will move within the stability triangle. If the center of gravity moves outside of the stability triangle, the truck will tip over. 1910.178 App A
 

Q: What is considered formal training?

A: Formal training is the combination of classroom and OSHA safety training, including lecture, discussion, videos, interactive computer learning or written material.

Sources

29 CFR 1910.178, Powered Industrial Trucks.

Occupational Health and Safety Administration (OSHA), Powered Industrial Truck etool.

(Rev. 5/1/15)

Find even more information you can use to help make informed decisions about the regulatory issues you face in your workplace every day. View all Quick Tips Technical Resources at www.grainger.com/quicktips.

Think Safety. Think Grainger.®
Grainger has the products, services and resources to help keep employees safe and healthy while operating safer facilities. You’ll also find a network of safety resources that help you stay in compliance and protect employees from hazardous situations. Count on Grainger for lockout tagout, fall protection equipment, confined space products, safety signs, personal protective equipment (PPE), emergency response and so much more!

DISCLAIMER:The information contained in this publication is intended for general information purposes only and is based on information available as of the initial date of publication. No representation is made that the information or references are complete or remain current. This publication is not a substitute for review of the current applicable government regulations and standards specific to your location and business activity, and should not be construed as legal advice or opinion. Readers with specific questions should refer to the applicable standards or consult with an attorney.

©2016 W.W. Grainger, Inc.