Danger Sign

Sign Up For Safety

Receive our free e-mail newsletters that are packed with insights and tips from safety experts. Want to make a difference in your company? Sign up today.

Tip: Sign Marking Requirements

Get important information about safety sign and marking requirements in the workplace.

Employers have a responsibility to warn employees, contractors, temporary employees and visitors about hazards that exist in the workplace. One of the easiest ways to accomplish this is to use and follow established safety sign and marking requirements.

Two agencies govern safety signs and marking: the Occupational Safety and Health Administration (OSHA) and the American National Standards Institute (ANSI). Under OSHA’s revised Hazard Communication Standard, organizations can now use either the ANSI standards from 1967-1968 (ANSI Z53.1, Z35.1 and Z35.2) or from 2011 (ANSI Z535.1, Z535.2 and Z535.5) for safety signage.

OSHA specifications for safety signs, accident prevention signs and safety tags are spelled out in 29 Code of Federal Regulation (CFR) 1910.145. These specifications cover all safety signs except those designed for streets, highways and railroads. These specifications do not apply to plant bulletin boards or to safety posters.

ANSI and the National Electrical Manufacturers Association (NEMA) have developed and published the ANSI/NEMA Z535 series of voluntary consensus standards for safety signs and colors. The ANSI/NEMA Z535 series is composed of six documents and a color chart:

  • ANSI/NEMA Z535 Color Chart
  • ANSI/NEMA Z535.1 Safety Colors
  • ANSI/NEMA Z535.2 Environmental Facility and Safety Signs
  • ANSI/NEMA Z535.3 Criteria for Safety Symbols
  • ANSI/NEMA Z535.4 Product Safety Signs and Labels
  • ANSI/NEMA Z535.5 Safety Tags and Barricade Tapes (for Temporary Hazards)
  • ANSI/NEMA Z535.6 Product Safety Information in Product Manuals, Instructions and Other Collateral Materials

Sign Classification and Requirements

OSHA has three classifications of signs:

  1. Danger signs – Indicate immediate danger and that special precautions are necessary. OSHA specifies that red, black and white colors are to be used for danger signs.
  2. Caution signs – Warn against potential hazards or caution against unsafe practices. OSHA specifies that caution signs must have a yellow background and black panel with yellow letters. All letters used against the yellow background must be black.
  3. Safety instruction signs – Must be used where there is a need for general instructions and suggestions relative to safety measures. OSHA specifies that safety instruction signs must have a white background, green panel and white letters. Any letters used on the white background must be black.

In the fall of 2013, OSHA endorsed the latest best practices related to safety signs by referencing the 2011 ANSI/NEMA Z535 safety sign and tag standards in its regulations.

The new sign and tag formats use nationally and internationally standardized elements to better convey safety messages in today’s workplace. New components include:

  • SAFETY ALERT SYMBOLSafety Alert
  • Indicates a potential personal injury hazard exists.
  • It is only used on DANGER, WARNING and CAUTION signs, labels and tags.
  • SIGNAL WORDS FOR HAZARD ALERTING SAFETY MESSAGESSignal Words
  • DANGER
  • Indicates a hazardous situation that, if not avoided, will result in serious injury or death.
  • Its use should be limited to the most extreme situations.
  • WARNING
  • Indicates a hazardous situation that, if not avoided, could result in serious injury or death.
  • CAUTION
  • Indicates a hazardous situation that, if not avoided, could result in minor or moderate injury.
  • Signal Words for Non-Hazard Alerting Safety Messages
  • NOTICENotice
  • Indicates information considered important but not directly hazard related (e.g., security, hygiene, equipment or property damage).
  • Signal Words for Instructional Safety Messages
  • SAFETY INSTRUCTIONSInstructions
  • Used to provide explanatory information like procedures and instructions.
  • More definitive words can be used in this signal word panel (e.g., LOCKOUT PROCEDURE).
  • SYMBOLSSymbols
  • Graphical symbols used to help bridge language barriers and draw attention to the safety message.
  • Specific shape, color and design principles are used to meet global compliance objectives.
  • TEXT MESSAGESDangerDanger Voltage
  • Carefully crafted text is used to convey the safety message to the intended audience in a clear, concise manner.

Employers can use either the ANSI standards from 1967-1968 (ANSI Z35.1 and Z35.2) or from 2011 (ANSI Z535.1, Z535.2 and Z535.5) for safety signage. This allows employers to use either the old or new format, and be in OSHA compliance.

 
Lettering Size

The wording on any safety sign should be concise and easy to read, according to ANSI Z535.2-2011, Section 8. The size of the lettering must be of a size that enables a person with normal vision, including corrected vision, to read the safety sign message panel text at a safe viewing distance from the hazard. The signal word letter height should be at least 50% greater than the height of a capital H in the message panel wording. The minimum safe viewing distance refers to the closest distance a person can be to the sign and still have time to follow the safety sign’s message to avoid the hazard.

Minimum Safe Viewing Distance (ft.) Minimum Letter Height for Favorable Reading Conditions (in.) Minimum Letter Height for Unfavorable Reading Conditions (in.)
≤4 0.16 0.33
6 0.24 0.50
8 0.32 0.66
10 0.40 0.83
15 0.60 1.27
20 0.80 1.68
30 1.20 2.51
40 1.60 3.36
60 2.40 5.04
80 3.20 6.72
100 4.00 8.40
125 5.00 10.49
150 6.00 12.58
200 8.00 16.79

 
Placement of Signs

Hazard alerting signs must be placed to alert and inform viewers from a safe viewing distance, according to ANSI Z535.2-2011, Sections 11 and 12. They must be legible, and must not be a distraction or create a hazard themselves. They must not be placed on or adjacent to moveable objects like doors, windows, etc. Safety and fire equipment signs must be clearly visible in the immediate vicinity of the equipment. Safety signs must be protected from damage caused by fading and other potential environmental conditions. Signs must be displayed with illumination or retro-reflectiveness as needed for adequate legibility under normal operating conditions. Where illumination is inadequate or colors are not recognizable, supplemental illumination must be used. Where illumination may be interrupted, the sign should be made with photo luminescent and/or retro-reflective materials, and/or equipped with emergency lighting.

Safety Color Coding

The following chart represents the color codes of both ANSI/NEMA Z535.1-2006 (R2011) and OSHA:

COLOR MEANING APPLICATION
Red Danger Safety cans and signs.
Stop Emergency stop bar or button on machinery. Identification of fire equipment.
Fluorescent Orange, Orange-Red Biosafety Labels and containers for blood and infectious waste. (Warning labels must be fluorescent orange or orange-red with the biosafety symbol in a contrasting color.)
Yellow Caution Tripping, falling and striking hazards. “Flammable, Keep Fire Away” labels on cabinets. Safety cans and containers for explosives, corrosives or unstable materials.
Orange Warning Parts of machinery or energized equipment that may cut, crush or otherwise injure. Inside of transmission guards for pulleys, gears, etc.
Green Safety Location of first aid equipment. Location of safety equipment, respirators, safety showers, etc.
Blue Information Signs and bulletin boards. Specific railroad warnings against starting, using or moving equipment being repaired.
Black, White, Yellow or Combination of Black with White or Yellow Boundaries Traffic or housekeeping markings. Stairways, directions and borders.
Magenta or Purple on Yellow Radiation Caution X-ray, alpha, beta, gamma, neutron and proton radiation.

 
Commonly Asked Questions
 
Q: Which requirements should be followed, OSHA or ANSI?
A: Where OSHA has specific requirements, they must be followed. In the absence of OSHA requirements, ANSI standards should be followed. Any applicable federal, state or municipal regulations must also be followed.
 
Q: Does OSHA specify what material type should be used for outdoor applications?
A: No. OSHA does not specify material types for sign applications. However, sign manufacturers do provide guidance on what material type will work best for your particular application. According to Brady’s sign material reference chart, fiberglass material will offer the longest average outdoor durability of 25 years, self-sticking vinyl signs will have an average 8-10 years, aluminum and self-sticking polyester will offer 5-8 years, and plastic signs will only offer 1-2 years of outdoor durability.
 
Sources

29 CFR 1910.144, Safety Color Code for Marking Physical Hazards

29 CFR 1910.145, Specifications for Accident Prevention Signs and Tags

ANSI/NEMA Z535.1-2011, Safety Color Code

ANSI/NEMA Z535.2-2011, Environmental and Facility Safety Signs

ANSI/NEMA Z535.3-2011, Criteria for Safety Symbols

ANSI/NEMA Z535.4-2011, Product Safety Signs and Labels

ANSI/NEMA Z535.5-2011, Safety Tags and Barricade Tapes (for Temporary Hazards)

ANSI/NEMA Z535.6-2011, Product Safety Information in Product Manuals, Instructions and Other Collateral Materials

Brady’s Material Selection Guide – Safety Signs

(Rev 11/11/15)

Find even more information you can use to help make informed decisions about the regulatory issues you face in your workplace every day. View all Quick Tips Technical Resources at www.grainger.com/quicktips.

Think Safety. Think Grainger.®
Grainger has the products, services and resources to help keep employees safe and healthy while operating safer facilities. You’ll also find a network of safety resources that help you stay in compliance and protect employees from hazardous situations. Count on Grainger for lockout tagout, fall protection equipment, confined space products, safety signs, personal protective equipment (PPE), emergency response and so much more!

DISCLAIMER:The information contained in this publication is intended for general information purposes only and is based on information available as of the initial date of publication. No representation is made that the information or references are complete or remain current. This publication is not a substitute for review of the current applicable government regulations and standards specific to your location and business activity, and should not be construed as legal advice or opinion. Readers with specific questions should refer to the applicable standards or consult with an attorney.

©2016 W.W. Grainger, Inc.