Arc Flash Label

Sign Up For Safety

Receive our free e-mail newsletters that are packed with insights and tips from safety experts. Want to make a difference in your company? Sign up today.

How to Read an Arc Flash Label

Here's a quick cheat sheet for reading an arc flash label

Arc Flash Label

1) Danger or Warning Header: A red “Danger” header is commonly used when the nominal system voltage is over 600 or when the incident energy is over 40 calories per square centimeter (cal/cm2). If less than either of these thresholds, an orange "Warning" header is typically used.

2) Arc Flash Boundary:  When an arc flash hazard exists, the shortest distance at which the worker—if not properly protected by flame-resistant clothing—may be permanently injured (the onset of a second degree burn or worse). The onset of a second degree burn on unprotected skin is likely to occur at an exposure of 1.2 cal/cm2 for one second.

3) PPE Hazard Category: represents minimum criteria PPE must meet to avoid onset of permanent injury if inside the arc flash boundary. Represented as category 1-4.4)    

4) Arc Rating of Clothing: Measured in calories/cm2, this rating measures the thermal energy at a working distance from the arc fault.

5) Incident Energy: The amount of thermal energy impressed on a surface, a certain distance from the source, generated during an electrical arc event and typically expressed in cal/cm2. Incident energy increases as the distance from the arc source decreases.

SHOP RELATED PRODUCTS

Equipment and Safety Labels
Equipment and Safety Labels
Safety Banners and Posters
Safety Banners and Posters
Label Makers, Printers and Supplies
Label Makers, Printers and Supplies

6) Working Distance: The distance between a person’s face and chest area and a prospective arc source.

7) Nominal System Voltage:  A nominal value assigned to a circuit or system for the purpose of conveniently designating its voltage class.

8) Limited Approach Boundary: An approach limit at a distance from an exposed energized electrical conductor or circuit part within which a shock hazard exists.

9) Restricted Approach Boundary: An approach limit at a distance from an exposed energized electrical conductor or circuit part within which there is an increased likelihood of electric shock due to electrical arc-over combined with inadvertent movement.

10) Arc-rated/Additional PPE:  Flash apparel, flame-resistant clothing, and other PPE that protect workers from hazards presented by an arc flash and/or shock.

11) Equipment ID: Identifies the piece of equipment that the warning label is associated with.

Banner

Find even more information you can use to help make informed decisions about the regulatory issues you face in your workplace every day. View all Quick Tips Technical Resources at www.grainger.com/quicktips.

Think Safety. Think Grainger.®
Grainger has the products, services and resources to help keep employees safe and healthy while operating safer facilities. You’ll also find a network of safety resources that help you stay in compliance and protect employees from hazardous situations. Count on Grainger for lockout tagout, fall protection equipment, confined space products, safety signs, personal protective equipment (PPE), emergency response and so much more!

DISCLAIMER:The information contained in this publication is intended for general information purposes only and is based on information available as of the initial date of publication. No representation is made that the information or references are complete or remain current. This publication is not a substitute for review of the current applicable government regulations and standards specific to your location and business activity, and should not be construed as legal advice or opinion. Readers with specific questions should refer to the applicable standards or consult with an attorney.

©2016 W.W. Grainger, Inc.