Injured Worker

Sign Up For Safety

Receive our free e-mail newsletters that are packed with insights and tips from safety experts. Want to make a difference in your company? Sign up today.

First Aid Kit Requirements

The Occupational Safety and Health Administration (OSHA) medical services and first aid regulation, 29 Code of Federal Regulations (CFR) 1910.151(b) states, "In the absence of an infirmary, clinic, or hospital in near proximity to the workplace which is used for the treatment of all injured employees, a person or persons shall be adequately trained to render first aid. Adequate first aid supplies shall be readily available."

The American National Standards Institute (ANSI) and International Safety Equipment Association (ISEA) American National Standard—Minimum Requirements for Workplace First Aid Kits and Supplies (ANSI/ISEA Z308.1-2015)—establishes minimum performance requirements for first aid kits and their supplies. First aid kits are classified based on the assortment and quantity of first aid supplies intended to deal with most types of injuries and sudden illnesses that may be encountered in the workplace. These may include major and minor wounds, minor burns, sprains and strains, and eye injuries. As each work environment is unique, it is expected that the contents of each kit will be supplemented as needed based upon the recommendations of a person competent in first aid.

The nonmandatory 29 CFR 1910.151 Appendix A refers to ANSI Z308.1-1998, Minimum Requirements for Workplace First Aid Kits. Since Appendix A was added, ANSI has updated Z308.1 many times. The most recent edition was approved on June 17, 2015, with an effective date one year from that date.

SHOP RELATED PRODUCTS

First Aid and Wound Care
First Aid and Wound Care
First Aid Kits
First Aid Kits

Topical Ointments, Creams and Antiseptics
Topical Ointments, Creams and Antiseptics

 

Classification of First Aid Kits

The newest ANSI/ISEA standard introduces two classes of first aid kits: Class A and Class B. Class A kits are designed to deal with the most common types of workplace injuries. Class B kits are designed with a broader range and quantity of supplies to deal with injuries in more complex or high-risk environments.

Below is a table listing the minimum required components for both Class A and Class B kits. The assortment and quantity of supplies included in the kits were chosen based upon reviews of workplace incidents requiring first aid treatment, similar international standards and current injury treatment practices. The quantity and size specifications given are the minimum necessary to comply with the 2015 standard.
 

Kits

The kit containers are classified by portability, ability to be mounted, resistance to water, and corrosion and impact resistance. Four types are identified:

Type I: Intended for use in stationary, indoor applications where kit contents have minimal potential for damage due to environmental factors and rough handling. These kits are not intended to be portable and should have a means for mounting in a fixed position. Some applications for Type I first aid kits are general indoor use, office use or use in a manufacturing facility. First aid cabinets would generally fall into this type.

Type II: Intended for use in portable indoor applications where the potential for damage due to environmental factors and rough handling is minimal. These kits should be equipped with a carrying handle. Some applications for Type II first aid kits are general indoor use, or use in office or manufacturing environments.

Type III: Intended for portable use in mobile indoor and/or outdoor settings where the potential for damage due to environmental factors is not probable. Kits should have the means to be mounted and have a water resistant seal. Typical applications include general indoor use and sheltered outdoor use.

Type IV: Intended for portable use in mobile industries and/or outdoor applications where the potential for damage due to environmental factors and rough handling is significant. Typical applications include the transportation industry, utility industry, construction industry and the armed forces.

Specific requirements for unitized first aid kits have been removed from the Z308.1-2015 standard to emphasize the importance of the contents rather than the configuration. Unitized kits contain first aid supplies in uniform-sized, color-coded boxes as follows:

• Blue – Antiseptic
• Yellow – Bandages
• Red – Burn Treatment
• Orange – Personal Protective Equipment
• Green – Miscellaneous

When deciding the class and type of kit that may be most appropriate, employers should consider the risks that are present and the potential severity and likelihood of an incident. Based on the number of employees, physical layout of the facility and the remoteness to emergency services, employers should also consider whether multiple first aid kits are needed. These considerations also come into play when determining if a kit needs to be supplemented with additional supplies. The selection of these items should be based on the recommendation of a person competent in first aid who is aware of the hazards faced and the number of employees at the worksite.

Maintenance and Inspection

To ensure the completeness and usable condition of all supplies, first aid kits should be inspected and maintained on a regular basis. Some supplies may have expiration dates; any that are beyond that marked date should be replaced.

Marking and Labeling

All labels and markings must be legible and permanent. Each kit and/or location must be visibly marked. Each kit must also have a label with the following information presented, as applicable, in at least a six-point font:

 

Frequently Asked Questions

Q: Is a consulting physician required to approve first aid supplies on site?
A: No. According to 29 CFR 1910.151, first aid supplies do not need to be approved by a consulting physician. They should, however, be selected by a person competent in first aid and knowledgeable of the hazards found in the specific workplace.
 
Q: Is it required that first aid kits be regularly inspected to ensure that contents are complete and up to date?
A: Yes. First aid kits should be regularly inspected to ensure they are full, in good condition and that contents that have expiration dates have not expired. The contents list for the first aid kits should be periodically reviewed to ensure that it meets the needs of the workplace and hazards faced at all times.
 
Q: Can over-the-counter medicine be put in first aid kits?
A: Over-the-counter medicine can be put in first aid kits if packaged in single-dose, tamper-evident packaging and labeled as required by Food and Drug Administration (FDA) regulations. Over-the-counter drug products should not contain ingredients known to cause drowsiness.

Sources for More Information

OSHA Medical Services and First Aid regulation, 29 CFR 1910.151

International Safety Equipment Association
1901 North Moore Street, Ste. 808,
Arlington, VA 22209-1762
Phone: 703.525.1695
www.safetyequipment.org

http://www.ansi.org/

(Rev. 7/2015)

Class A

Find even more information you can use to help make informed decisions about the regulatory issues you face in your workplace every day. View all Quick Tips Technical Resources at www.grainger.com/quicktips.

Think Safety. Think Grainger.®
Grainger has the products, services and resources to help keep employees safe and healthy while operating safer facilities. You’ll also find a network of safety resources that help you stay in compliance and protect employees from hazardous situations. Count on Grainger for lockout tagout, fall protection equipment, confined space products, safety signs, personal protective equipment (PPE), emergency response and so much more!

DISCLAIMER:The information contained in this publication is intended for general information purposes only and is based on information available as of the initial date of publication. No representation is made that the information or references are complete or remain current. This publication is not a substitute for review of the current applicable government regulations and standards specific to your location and business activity, and should not be construed as legal advice or opinion. Readers with specific questions should refer to the applicable standards or consult with an attorney.

©2016 W.W. Grainger, Inc.