LOTO

Sign Up For Safety

Receive our free e-mail newsletters that are packed with insights and tips from safety experts. Want to make a difference in your company? Sign up today.

Are the Arc Flash Hazards in Your Workplace Properly Labeled?

A common practice for keeping employees safe, arc flash labeling helps companies inform workers about potential electrical hazards in the workplace.

Equipment labels play an important role in keeping workers well informed and safe while they’re working in and around energized equipment. In an effort to minimize the occurrence of arc flash incidents, the National Fire Protection Association (NFPA) outlines important labeling rules in NFPA 70E as follows: 

  • Safety signs, safety symbols, or tags must be used (where necessary) to warn employees about electrical hazards that might endanger them.
  • These signs and tags must meet the requirements of the applicable state, federal, or local codes and standards.
  • Safety signs, tags, and barricades used to identify energized “lookalike” equipment can be employed as an additional preventative measure.
  • Arc flash labels must contain the nominal system voltage, arc flash boundary and at least one of the following:
    • Available incident energy and the corresponding working distance, or the arc flash PPE category for the equipment, but not both
    • Minimum arc rating of clothing
    • Site-specific level of personal protective equipment (PPE)

SHOP RELATED PRODUCTS

Equipment and Safety Labels
Equipment and Safety Labels
Safety Banners and Posters
Safety Banners and Posters
Label Makers, Printers and Supplies
Label Makers, Printers and Supplies

Addressing the Hazards

Electrical equipment such as switchboards, panelboards, industrial control panels, meter socket enclosures, and motor control centers that are likely to require examination, adjustment, servicing, or maintenance while energized must be properly labeled with an arc flash label to maintain the highest levels of safety.

The information displayed on the label should only be present based on the method used to determine the arc flash risk. If the arc flash PPE category method is used, for example, then only the PPE category (1-4) should appear. And if the incident energy analysis method issued, then the incident energy (cal/cm²) should appear.  

All calculations and data on the label must be documented to support the information on the label. The data shall be reviewed for accuracy at intervals not to exceed five years, and the owner of the electrical equipment is responsible for the documentation, installation and maintenance of the labels.

As you review your facilities and identify any arc flash risks, be sure to label them in accordance with NFPA 70E and in a way that employees will understand and respond to.

 

Banner

SOURCE

National Fire Protection Association, NFPA 70E, Standard for Electrical Safety in the Workplace

Find even more information you can use to help make informed decisions about the regulatory issues you face in your workplace every day. View all Quick Tips Technical Resources at www.grainger.com/quicktips.

Think Safety. Think Grainger.®
Grainger has the products, services and resources to help keep employees safe and healthy while operating safer facilities. You’ll also find a network of safety resources that help you stay in compliance and protect employees from hazardous situations. Count on Grainger for lockout tagout, fall protection equipment, confined space products, safety signs, personal protective equipment (PPE), emergency response and so much more!

DISCLAIMER:The information contained in this publication is intended for general information purposes only and is based on information available as of the initial date of publication. No representation is made that the information or references are complete or remain current. This publication is not a substitute for review of the current applicable government regulations and standards specific to your location and business activity, and should not be construed as legal advice or opinion. Readers with specific questions should refer to the applicable standards or consult with an attorney.

©2016 W.W. Grainger, Inc.